Diagnostic Messages and Notification Display

Geo SCADA Expert provides various mechanisms for reporting diagnostic information.

During day-to-day operation, Geo SCADA Expert logs activities via:

Additionally, you can ascertain the status of an individual item in the database by viewing that item's Status Displays.

Other displays, such as Trends and Mimics, also provide information about system activity and status.

Additionally, if Geo SCADA Expert is unable to complete a user-instigated task, such as Control request, diagnostic information might be provided in the form of a pop-up ('modal') message dialog box.

During system configuration, Geo SCADA Expert reports diagnostic information using a variety of additional mechanisms. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Additionally, icons in the Database Bar are overlaid with a red 'X' if they contain invalid configuration (for more information, see Correcting Invalid Configuration).